I am trying to drive a high power LED. It is 0.240A when at max power.
Is it possible to use in parallel two pins of the TLC5940 chip to drive it. It would be most convenient for several reasons. I could switch the two channels up pretty much in sync to avoid problems with reverse current etc. This can be done over time. The work isn't a fast application.
Thanks