This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Active PFC for variable load with peak of 2,5kW 360V DC output

Other Parts Discussed in Thread: UCC28070

Hello,

I am junior power designer, still at learning state. I will be glad if you could  recommend me design (part) which will be able to provide steady 360V DC output with variable load up to 2,5kW. I tried to use UCC 28019 but to use it on lower loads i need to have large coil (with peak current about 20A, and large inductance, coil will be really huge). With minimal calculated inductance used , PWM output works with audible noise on coil (probably few Hertz). Aprox after reaching 200W load buzzing is away.

So i need probably to use higher inductance boost coil, which will be so huge...

Or different design - > faster PFC?

Can you please reccomend me something? Thanks