Other Parts Discussed in Thread: BQ25798
Hi,
We have designed product using the BQ24179 using a standard USB charger on one port and a solar charger on the 2nd port. When we use the solar charger the input voltage will drop when the sun is blocked and eventually we will be in a "poor source" state. Once the sun comes back out again the charger does not move out of this "poor source state" even though the input voltage is high enough. So the charger is stuck in this "no charging state".
I have read "8.3.5.2 Poor Source Qualification" and this makes sense why this occurs. Does TI have a suggestion on how to handle this situation? I could clear the EN_HIZ bit every 5mins or so to start the qualification cycle again, but I don't like the idea of waking up a system every 5 mins which may already be low on power. Is there a better solution which would at least trigger an interrupt when voltage was high enough so I can start the qualification again?
If polling is the only answer, then would you have a list of recommended alternatives for a charging chip? We need to have alternatives which are available for a build in the next month or so, so I assume this limits us a little as well.
Thanks for the help,
Chris