This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28951: CC/CV MODE FULL LOAD ISSUE

Part Number: UCC28951
Other Parts Discussed in Thread: UCC28950,

Dear Sirs

 I cannot achieve my expected output voltage and current with the Tina model, could you help suggest how to adjust circuit parameter?

Vin:500V

Vout:14.4V

Iout:278A

The Tina model is shown below

UCC28950 and UCC28951 TINA-TI Steady State Reference Design Current doubler.TSC