Hello, I'm Marco from Italy. I have a board designed with this part, LMR33640, I've already put it in production last year, and is a functional board, tested and approved. Problem is that the part is not available. There is some alternative part that have the same pinout and the same external components configuration?
Here is my system configuration:
-Vin: 14~24 Vdc
-Vout: 12Vdc
-Max output current: 2A
Then i need something compatible, firstly for the pinout that can't be changed, dued to already existing board.
Thanks a lot, Marco