This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
I simulate the TPS62812-Q1 using PSpice for TI in order to generate a 3.3V and simulate a load transient.
From the simulation seems that the converter isn't stable in steady state condition but I followed the dataseet indication for all the external parts.
Could you check please if there is an error in my simulation ?
Attached you can found a pdf with schematic and waveform result.
TPS62812Q1 PSpice simulation.pdf
Thanks and Best Regards
Matteo
Hi Matteo,
The input voltage set for quite frequent that's the reason output voltage oscillating lot. I would suggest to increase supply pulse width higher to see device performance.
Schematic looks according to datasheet recommendation and I don't see critical issue there.
Best regards,
Tanvee
Hello Tanvee
After different trials, I verify that the issue is the maximum step size in the transient options.
The previous simulation was done with a maximum step size of 50ns, but reducing it the simulation is more accurate but require more time.
Attached the result with a maximum step size of 0.5ns, there are no oscillation in the output voltage at steady state.
TPS62812Q1 PSpice simulation 2.pdf
Best Regards
Matteo
Hi Matteo,
Thanks for sharing the details.
Simulation results look okay to me.
Best regards,
Tanvee