Part Number: TPS61181
Hello,
I have a customer with a question on PN: TPS61181
According to the datasheet, this product has a Vbat input voltage range of: 5 to 24V.
However, it also lists the absolute maximum Vbat range as 24V.
The customer has a 24V battery with a 3% tolerance, which can reach just under 25V.
They would like TI to confirm that this product line has no tolerance between normal input range and absolute maximum input, or if their battery is acceptable.
Thank you,