Other Parts Discussed in Thread: BQ25170, BQ24040
After my battery is charged, is there a way to hold the battery at full charge? Do I have to disable and enable the charge pin or can I keep the charger in constant charging so it keeps the battery from discharging once the timer timeout is complete? TM_SEL pin seems to suggest that the max time for the charger is 6 hours. What if the user keeps the device on a dock and the charger time expires.