Part Number: TPS7A47
Hi Team,
Usage conditions: TPS7A4701, Vin=24V, Vout=22V
I'd like to lower value of Feedback-divider resistance(R1 and R2) in order to avoid Vout reduction.
1) Is it OK to R2 is 1kΩ?
*10kΩ is recommended in the data sheet but 1kΩ can keep the current through R2 over 35uA.
*R2 ≥ 1.4V/35uA = 40kΩ

2) Is there lower limit of R2?
Best Regards,