Other Parts Discussed in Thread: EV2400, BQSTUDIO
Hello,
We are using the BQ76952 cell management IC to balance and protect a custom lithium ion battery pack. There are a total of 14 Panasonic 18650 cells within the pack. The Bq76952 is configured to balance and protect the pack independently of a host. There is a PIC microcontroller that is powered by the LDO reg 1 (3.3V) and is connected to the I2C bus to collect data on cell voltages when required.
The BQ76952 was configured and all the basic tests (cell undervoltage, cell overvoltage, cell balancing, thermal shutdown, overcurrent, short circuit) were tested and successfully worked at the correct limits. However, 8 packs was left sitting on the shelf in sleep mode for a month and all the cells drained to 0.3VDC. After they were set to sleep, the regulator REG1 was checked and it was disabled (0 VDC).
Do you have any ideas why the cells would drain completely? Attached is a copy of the schematic and the config file that was used for the BQ76952.
Thank you,