I have an application that needs to drive ~ 70 incandescent bulbs, Vbulb = 28V and IBulb is 30mA nominal. Bulbs are backlights for lots of buttons. The solution being replaced is discrete FETs and many other components. The biggest issue - As the bulbs start to fail (and they do) the nominal resistance of the filament goes down and the drive current if unchecked goes through the roof. At which time the bulb usually fails open.
Would this be an appropriate application for the TLC5947 ? (or is this just a bad idea)
Single bulb per output, Vbulb/led = 28Vdc
Ilim set to 30mA
Software would use 0% and 100% settings for PWM
Concerns -
Will the part maintain current limit as bulb parameters vary ?
Will an almost shorted bulb damage the TLC5947 ?
Thanks.