Hi Amiel,
Hope you're doing good, and happy thanks giving day!
Currently I'm using TI c2000 controller(F28002x) device to control PFC in primary side, and UCD3138 in secondary side to control LLC.
Now I'd like to update primary side MCU's firmware via PMBUS interface, this requires to send data to UCD3138 by Pmbus firstly, then UCD3138 translate it into UART and send it to primary side MCU. But currently UCD3xxx Device GUI only support to parse UCD3xxx devices' hex/x0 file, can you help to add customized boot options on GUI that users can configure what range of memory to be parsed and download?
In addition, if using fusion API to realize this feature, which examples can be used as start point to realize this feature?
And the fusion API user guide released by TI is written in about 10 years ago, is there a new version that can be shared with TI users?
Thanks,
Jack