This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25118: RE : Submission for Design Review

Part Number: LM25118


Design Requirements:

Input Voltage Range: 9V - 36V

Output Voltage: 28V

Output Current: 2.8A

Max Allowable Voltage Ripple(peak to peak): 100mV

Find the attachment below that contains the design file for the above requirement submitted for the TI review and share the comment for the same

sch_501-1-02018_lm25118.zip

  • Hi Jayakrishnak,

    the schematic looks good but please double check the rating of the output caps. When using ceramic or MLCC there is a DC bias derating where the effective capacitance could be much lower. So the current used capacitance on the output might be too low.

    Also ensure the RMS and Saturation current of the inductor are dimensioned well.

    Best regards,

     Stefan

  • Hi Jayakrishnak,

    I have not seen an update for the last 24 days, so I assume the questions are answered.
    I close this thread now. If there is still something open reply and the thread will get open again.
    If you have any other question or of the thread gets locked, please open a new one.

    Clicking the Resolved Button also helps us to maintain this forum.

    Best regards,

    Stefan