Other Parts Discussed in Thread: LM5020, UC1843,
I am working with a power supply project. The project has two power module which switching frequency must be between 400kHz ~ 600kHz.
module 1 : Vin 20V~34V ; Vout : +5V/16A -5V0.5A
module 2 : Vin 20V~34V ; Vout : +5V/3.5A -5V0.5A +15V/0.5A
The topology has not been selected,forward , flyback and others? The control IC should be selected from LM5020/5025/5026/5030 or other UC1843, UC1525.
Can TI suggest some solutions? Thanks.