Part Number: TPS40304

We are using the TPS40304 for a 15V to 3.3V (0.5A to 5.5A) converter. Our design analysis values closely match the webench design values shown in the schematic below. I’ve included a scope capture of the M2 drain waveform. Output is regulating at 3.3v over load range and line between 14 and 16v. Ripple doesn’t look too bad at approximately 50mvpp but frequency at about 100khz, not 600khz as expected. Can you give me an idea what may be causing this….or what mode of operation the chip may be in? It looks like two 600kHz switch pulses, every 100kHz (about 7.5usec between cycles).