Part Number: LM5116
Other Parts Discussed in Thread: LM5121, LM5122, LM5143
I would like to use 2 of the LM5116 control devices to create a 2-phase Buck converter. I have the 2 clocks that are 180 out phase. I was initially just going to connect the FB pins of the two devices together, but I think that will cause a problem. Is there an established way to connect the two devices together? Can I instead tie the Comp output pins together? this is the idea in a very simplistic block diagram.