Hello,
My customer is using LP38690SD-3.3/NOPB for the optical module application.
The following defect occurred in LP38690SD-3.3/NOPB while using the optical module.
- Input voltage = 5V, Typical load current = 230mA
- The output voltage of the LP38690SD-3.3/NOPB has been lowered to 2.4V~2.7V.
- When the load is removed, the LP38690SD-3.3/NOPB output returns 3.3V.
- When power is suppied from an external device, the load is normal.
- When replacing with a new LP38690SD-3.3/NOPB, the module becomes normal.
Is it possible that the above symptom is caused by damage to the LP38690SD-3.3/NOPB?
Please advise on what issues could be causing the above failure symptom on the LP38690.
Thank you.
JH