Hi,
I recently bought the evaluation board TPS92010EVM-592 and it works fine, so I tried to build my own bord using a circuit that you have in the users guide but for some reason it didn't work, the document is "sluu418c.pdf", I downloaded from this link http://www.ti.com/litv/pdf/sluu418c, I bought all components that the document asks for, except the mosfet because I coundn't get it because of delivery times, so I replaced it with STD3NK80ZT4, which is the only diference between the two boards but in the board I made the maximun voltaje that I get is 12.7V with a 100mA load and 17.3V without load, I tested all configurations of constant current that the document says but the problem still continues, I got little variations between the differents configurations but nothing relevant. Also the efficience is bad, it is arround 62%.
Can any one make me some recomendations about it? or Does anybody know how to solve this? I will appreciate any suggestion.
JC