This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24193: Alternatives to BQ24193, ideally with JEITA compiance

Part Number: BQ24193
Other Parts Discussed in Thread: BQ24292I, BQ25672, BQ24192, BQ25892

The sourcing situation for BQ24193 is difficult. We are therefore looking for alternative parts. Preferred is something pin compatible. 

1. Is BQ24193 the only JEITA compliant option in the BQ2419x family?

2. Is there some sort of simple side-by-side comparison table for the options in this series (that we assume largely pin compatible)?

3. If there is no pin compatible option with JEITA compliance, so that a PCB redesign would be an option (still with the same size IC to fit), would any of you have advice on which way to look? I2C control is still required, and charging of a single cell up to 4.35V, with at least the same level of absolute max Vin as BQ24193 (22V).

4. If JEITA compliance is disregarded, would BQ24292I be the suggested replacement to stay close to BQ24193 and lower the sourcing risk?