Dear Support,
After the first programming of the device (I made sure not to lock the EEPROM) now when the device starts, it reports:
SEVERE_ERR_INT and FSM_ERR_INT errors.
The rails have outputs and I can read all the registers however, when I even write into just one register the device stops communicating.
When I try to re-program the device the same thing happens, during programming the nINT LED turns off and the device becomes disconnected from the AEVM Controller.
Thanks,
Lauri