Other Parts Discussed in Thread: LM2940-N, LM2941, TPS7B86-Q1, TPS7A94, TPS7A20, TPS62175
Hi, TI expert.
A customer has an inquiry about a replacement for the LM317MKVURG3 (TO-252 package).
- SPEC : DC24V -> +5V, 500mA
A customer is using it with the above specifications, but since it is a TO-252 package, it occupies a lot of space on the PCB and a MORS resistor has been added to the input stage due to the problem of generating a lot of heat.
As an alternative, if there is a device suitable for Energy Star in a small package size, please recommend it.
Please check. Thank you.