Part Number: UCC39002
Hi Experts,
I want to load share with two LDO regulators using UCC39002. The input power voltage of LDO regulator is DC 12.8V. And the output of LDO is 12V. The current of one LDO is 12A. The shematics is attached. Please help review whether the schematics is correct and caculate the values of resistors and capacitors of UC39002 circuit. Thank you!
Best Regards,
Wells