Part Number: UCD90120
Other Parts Discussed in Thread: UCD90320, UCD90240, UCD9090A, UCD90160A,
I read this app note which says,
Another method to cascade multiple devices is to connect the power-good output of the first device to a MON/GPI pin of the second device; connect the power-good output of the second device to a MON/GPI pin of the third device, and so on.
and later on in the same paragraph,
Optionally, connect to the GPI pin instead of the MON pin if the UCD9090A, UCD90160A, UCD90240, and UCD90320 devices are used in the cascading method to save the MON pin for other uses.
However, does this mean that GPI can't be used at all for the power good input to the first sequencer if it were an older device such as the UCD90120 (which we're using due to supply chain issues)? Granted, it doesn't have the Fault Pin feature, but assuming we don't require that in our application I don't see why it can't just go to the GPI pin regardless. See image below for the configuration I'm referring to. I would very much like to free up that MON pin ;)

Cheers, Adrianna