This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS929120-Q1: Current accuracy @75mA ?

Part Number: TPS929120-Q1


Hi 

If we set the output current 75mA, is it correct the current accuracy is +/-5%?

And the worse case the output current may go up to 75mA x (1+5%) = 78.75mA ?

  

  • Hi PY,

    Correct, the output current accuracy for 75mA setting is +/-5% which means that the current could maximum reach 78.75mA. You can for example see Figure 6-6 in the datasheet where at lower supply voltage the current is a little higher, but at the maximum supply voltage the current is a little lower. Under any condition mentioned in the datasheet (e.g. supply voltage range, temperature range), the accuracy will stay within this range.

    TPS929120-Q1_datasheet_Fig6-6