Hi Team,
My customer is considering use LMR43610MB3RPER, could you kindly help with following questions?
1. Does the parameter "IPEAK-MIN" means the current when control mode switches between PFM and PWM mode?
2. What is max ON duty of HS switch? Should we refer to Dmax below or can we calculate it from ton-max/(ton-max+toff-min)=13us/(13us+85ns)=99.35%?
3. Customer wants to compare power efficiency with other device for Vin=12V, Vout=5V. Is there graph available like following?
Thanks.
Regards,
Jo