This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need EOS and Gas Gauge for constantly charge-discharge solar system

Other Parts Discussed in Thread: BQ34110

I need advice for choosing IC for solar powered autonomous system.  Our system charge battery and power the device in the day and battery discharge for powering device at night. aprroximately this use 20% of lead acid baterry capacity (100ah). Charge to 100%  in daylight  discharge to 80% at night.  How i can track the health of battery and determine EOS state? Battery works every time and never rest. 

Best regards.

Artem.