This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RSOC in bq78PL114

Other Parts Discussed in Thread: BQWIZARD

Hi All!!!

I have bought pl114EVM and connected 8S cells simulator with 10 Ohm resistors. I use bqWizard software for communicating with the cells. I checked all the safety parameters, SMBus communication etc... EVERYTHING seems to be fine, except that , the RSOC alone is always showing 0%. I calibrated the temperature to be 25 deg C. If i give anything for current calibration, the RSOC changes to either 54% or 6% and remains the same even if the BAT vge is reduced or increased. Guide me if the current calibration that i do is wrong....