Hi,
are there any issues using an external 10K pullup (to a LiIon battery) on the D1 logic input of the TPS2115A? the LiIon battery will be one of the two power switch inputs (IN1) to this mux.
Thanks,
Sal
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
are there any issues using an external 10K pullup (to a LiIon battery) on the D1 logic input of the TPS2115A? the LiIon battery will be one of the two power switch inputs (IN1) to this mux.
Thanks,
Sal
Hello Sal,
The D1 pin already has an internal pull-up; however, using a 10kΩ external pull-up to your LiIon battery is fine too.
Regards,
Kalin Burnside