Hi,
I want to use the LMR38020 to make several power supplies on a board and I would like to synchronize them all and set them to 300Khz. Is it possible to use the same synchronization signal coming from a microcontroller (F28388DZWTS) to make it, if yes do you have a schematic to propose me?
If I make the diagram below I imagine that I disturb the adjustment of the frequency because the 2 resistors of 88k7 (300khz) are in parallel!
Should I put only one resistor Rt which will be shared by each component or should I have only one synchronization signal per component?
Best regards