This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Need help:
Hello,
Firstly, I have reviewed the schematic, output capacitance value looks out of the range of LC matrix to what is recommended in the datasheet.
You have more than 100uF capacitance at the output whereas 10uF is the most recommended value in the datasheet with 2.2uH inductor for voltages greater than 1.8V at output.
I have few questions to dig deep into the issue.
1) Can you share which inductor (part number) you are using?
2) Just to confirm that I have understood it right, damage is happening at customer's side?
3) Is there any failure analysis performed by you already on damaged devices?
4) Can you provide detail info about the end equipment?
You can also contact by an email or send me a private message if there are confidential reasons.
Thanks and Best Regards,
Farheen
Hello Simba Su,
Do you have any further question related to this thread?
Thanks and Best Regards,
Farheen
Hello Simba Su,
I am closing this thread for now. If you have any further request related to this thread, please feel free to open it by commenting below.
Thanks and Best Regards,
Farheen