Hi,
i am powering BQ25150 from battery (own standalone pcb without I2C connections).
1) When pressing /MR line down for a period battery voltage is seen on PMID. However, LS/LDO output is showing 0V.
2) When powering same pcb from VIN LS/LDO is powered to 1.8V.
3) On battery powered case, when i set /LP line "HIGH" temporary or permanently, LS/LDO output startsup to 1.8V. When pulling "LOW" again /LP line LS/LDO keeps 1.8V.
Only removal of the battery will set BQ25150 back on step 1) again.
What could explain this behaviour? My previous PCB with some small differences LS/LDO starts up normally from battery only as well without need of /LP "HIGH"