I have dual battery packs of between 10.5 14.5 voltage.
I want to power up with pack A if it is available, then when the voltage drops below 10V, (Battery exhausted or removed) seamlessly switch to pack B. Pack B should remain as priority even if pack A is replaced. When Pack B drops below 10V, it should seamlessly switch back to A.
As a bonus it would be great if I could disable both packs in the same device for shutdown.
Is this possible with any of the TI power ORing products?