This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear team,
According to the equation 9 in the datasheet, Rcomp=88k. My customer finally choose 100k & 820pF< is it ok?
Thanks & Best Regards,
Sherry
Hi Sherry,
1. It depends. Note that when you calculate the compensation network you need to use effective output capacitance. If you have RCOMP < 120 kΩ and CCOMP> 820 pF you can recommend the parameters to customer.
2. It seems that there are may output capacitors. Make sure customer really need them.
Hi Yichen,
Please help recommend the Rcomp and Ccomp based on customer's condition, thanks.
Best Regards,
Sherry