This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5010: What may be the problem with my design?

Part Number: LM5010


Hi, I'm trying to use the LM5010MH/NOPB to convert input voltages in the 24V to 48V range down to 15V.
Currently, it can only output up to about 3.5V.

Here is the schematic for my circuit.
I've also attached the Webench design that the implementation above was based on.

Any thoughts or ideas for troubleshooting?