This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2673: Current limit adjust

Part Number: LM2673


The datasheet recommends Iadj > 1A. But we have configured 0.99A, using 37.4K, 1% resistor. Can you please specify what problems can be be expected, or its fine to use 0.99A. The max avg load current is 0.4A. Input voltage is 15V regulated and output voltage is 12V. Inductor is 33uH.