Hello, guys.
We need to drive the PTC Heater element that has a rated voltage of 12V and temperature of 70C as you can see below.
We are experiencing a high inrush current (above 4A) during the initial few seconds when we start the system (e.g. turn on the 12V power supply switch).
What would be the best way to protect the system from that inrush current?
We used LM317 configured as a current limiter in series with the PTC element with the idea to limit the current to 1.2A. The system seems to work well, the initial current is not above 1.2Amps but we have a side effect of heat dissipation on LM317 (temperature on LM317 can go up to 100C).
Is there any better way? Perhaps to use some load switch with adjusted rise-time or even buck-boost regulator (e.g. TPS552882) that will give us 12V output in a configuration where the current will be limited to ~1.2Amps.
I noticed that some of your PWM motor drivers (e.g. DRV2510) have optional second-order Butterworth low-pass filters with the purpose of limiting peak current (see image below). Would that help in our case?
Thanks in advance for your time and efforts. Looking forward to reading from you.
Sincerely,
Bojan.