Dears,
LM5176 is used in DC to DC 40W, the specifications are as follows
DC input: 12V ~ 50V
DC output: 16V / 2.5A
At present, when the IC is controlled in the buck-boost region, the LM5176 will be damaged. Please help confirm the problem. The description is as follows:
1. When DC input 12V (boost mode), output 16V/2.5A works normally.
2. When DC input 24V (Buck mode), output 16V/2.5A works normally.
3. When DC input is between 15V~19V (buck-boost region), LM5176 will be damaged (Pin26 BOOT1 and Pin28 SW1 low impedance)
I have checked the waveforms in the buck-boost mode, the Vgs was stable, and also choose the low Vth and Qg MOSFET, but the IC will be damaged after working for a period of time.
Has TI ever encountered this similar problem? Is there a solution?
Thanks and regards.