Other Parts Discussed in Thread: LM5170
I seted the the frequency=100K, but i can not measure the freuency?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,EM
Thanks for yout help. I can get the 100kHz of the gate pin . but there is not right issue?
when apply DC 48V to the HV port, the LV port will get the 20V and i try to adjust the voltage of ISETA pin
from 0~1.25v, the LV port voltage can not change, what can i do next?

Hi,EM
Thanks for yout help. I can get the 100kHz of the gate pin . but there is not right issue?
when apply DC 48V to the HV port, the LV port will get the 20V and i try to adjust the voltage of ISETA pin
from 0~1.25v, the LV port voltage can not change, if LV is in the OVP mode?
also we check the wave of the HO2 wave, this is different with the datasheet.
...
Hello,
Thanks for your feedback. Let me reach out for the expert of this device for further support, we will come back to you as soon as possible.
Kind regards,
EM
This is complete sch, there are a few question need to help:
1. when power on the LM5170 board , the LV port voltage about is 20v, can i set the LV voltage to 14.8v?
2. The HO1/2 wave is not pwm wave and different with the datasheet, if it is ok?
3. Can set the ovpA protect voltage to 15v, Now the LM5170 chip very easy damage by LV high voltage.
4. If the LM5170 have the OCP protect?
Hi Wenwu,
I think we have your other post question covered here so I'll just close the other one.
For your questions, I'll need a few more information.
1. Could you please help me identify the ISETA connection on the schematic? It is tied to "FB" but I cannot find FB elsewhere.
2. As mentioned in the other post, could you please show where you probe (or which two points you probe) on the board for this waveform? You can mark them on the schematic as well.
3. What is the LV high voltage?
4. LM5170 has the cycle-by-cycle current limit protection. You can refer to the datasheet for more details.
Thanks,
Yinsong