Charger IC : BQ24610
Battery : 8.4V(normal 726V) / 14.7A . ( 2S3P. INR21700)
If charge up to 90%, I want the battery to finish charging and charging-complete -LED turn on.
Viset2 : 1.4A
If Viset2 : 1.4A, → If 0.9C is charged, is it charing-Complete state?
If Viset2 : 1.4A, is it SAT1:0 / STAT2:1?