Hello,
I am trying to simulate a LLC converter using UCC256403 in SIMPLIS, in the transient model it states HV pin, VCC pin, BLK pin, BW pin, RVCC pin, HB pin, and HS pin are not emulated in this model. Does that mean those pin are not available in the model to simulate or that the transient simulation was constructed without using those pins? I am trying to build a circuit with 12V input with 6V and 4A output. So far using the design calculator, I haven't been able to successfully simulate the model.