Hello,
My customer is using LMR36510ADDAR under the conditions below.
- VIN=48V / VOUT=5.1V / Inductor=4.7uH / COUT=10uF/16V/1608/+-20%/X6S
If the capacitance of COUT changes because the COUT capacitor's temperature rises above the guaranteed operation temperature,
does an error occur in the LMR36510 VOUT voltage level or output noise?
Thank you.
JH