This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54J061EVM: switching behavior between 6kHz and 2MHz

Part Number: TPS54J061EVM


Hi team,

I noticed some behavior shown in the below,  the test condition is transient 0.01A to 0.5A in 2MHz.

But instead of scatter pulse which behave normally in the 600kHz picture, it appears a group of dense switching pulse in the light load DCM mode in the 2MHz condition.

why does this happen ? does it somehow trigger back to CCM and operate in 2MHz?

2MHZ                                                                                         Zoom-in

600KHz

Regards,

Fred