This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV751: TLV751180330PDSQR Enable input when not powered

Part Number: TLV751


From the datasheet the enable signals (pin3 and pin5) of the TLV751180330PDSQR are both active high.

I am driving the enable signal with an push-pull output of a microcontroller.

I would like to know if the input voltage (pin 9 and Pin 6) are removed from the TLV751180330PDSQR , can I still drive the enable signal high without any issues when the microcontroller is still powered.