Hello,
Please provide below data in the table
Part Number | Kcl Min | Kcl Nominal | Kcl Max | Vcl Min | Vcl Nominal | Vcl Max |
TPS4H160-Q1 | ||||||
TPS2H160-Q1 | ||||||
TPS1H100-Q1 |
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Please provide below data in the table
Part Number | Kcl Min | Kcl Nominal | Kcl Max | Vcl Min | Vcl Nominal | Vcl Max |
TPS4H160-Q1 | ||||||
TPS2H160-Q1 | ||||||
TPS1H100-Q1 |
Hi Vishwas,
For these devices we only specify the nominal K_CL.
TPS1H100-Q1 is specified at 2000 while TPS2H160-Q1 and TPS4H160-Q1 is specified at 2500.
Then to find the bounds, use the current sense accuracy numbers to get the bounds of K_CL at the specific current load that you are trying to sense.
For example for TPS1H100-Q1 at 0.5A, you will see a +- 20% range which makes that K_CL_min at 1600, nominal at 2000 and max at 2400.
The V_CL(th) number does not shift significantly across the operating range and so the limiting factor for this calculation is the K_CL variation. The ILIM resistor variation will also add to the inaccuracy.
For more information on current limiting, we recommend looking at this app note: https://www.ti.com/lit/an/slva859b/slva859b.pdf
Thanks,
Shreyas