Other Parts Discussed in Thread: BQKEYPROGRAMMER
Hi,
We're using the bqKey Packager and bqKeyProgrammer software to program BQ40Z80 ICs with an ECC key but are getting the below error.
A few seconds after attempting to program the key, the error "Key Programming Failed!" is displayed with the comment "Validating ECC challenge response failed. Retry this operation" at the bottom of the window:
These are the settings we're using to generate the key (example values used as we do not wish to share the actual keys!):
This seems to follow the guidelines set out in SLUUBU3 but we're not able to get the key programmed onto the BQ40Z80? We have managed to use this software to program an SHA-1 key but we need to use the more secure ECC option.
We've tried both the 4800_0_04 firmware and the 4800_0_02 firmware on the BQ40Z80 with no luck. We've also tried multiple BQ40Z80 ICs with the same result. Are there any other steps that we're missing that aren't detailed in SLUUBU3 document - it's not particularly detailed?
Also please could you confirm the software does work with the BQ40Z80 on both 4800_0_04 firmware and the 4800_0_02 firmware? When opening the software the word 'TEST' is displayed - is this still development software, is it fully functional?
Thank you in advance. The rest of the fuel gauge seems to be working well, we'd just like to add this final authentication feature.
Thanks
Matt