This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM1117: LD1117DT12CTR replacement request

Part Number: LM1117

Hi team,

My customer want to get the recommend LDO socket to replace LD1117DT12CTR.

Could you please help to check that? thx

  • Hey Chen,

    Your device LD1117DT12CTR is an 800mA, 1.2V LDOin a 3 pin DPAK (TO-252)

    We do not have any P2P options with this output voltage to directly replace this device but we have some similar devices in different packages with adjustable output volatge

    The best crosses I would recommend are:

    TPS78512QKVURQ1 -1A, 1.2V, 5 pin DPAK

    TLV76701DRVR -1A, ADJ, 6 pin WSON

    Thanks,

    -Jimmy