Other Parts Discussed in Thread: LM5156, , LM5155, LM5155EVM-BST
Hello Sir / Madam,
I need a DC-DC booster for cooling Fan loading in EMI dummy load box.
I have 54V cooling fan and the AC - DC power supply with 12V output.
so, I want to design a DC DC booster from 12V input and 52V output ~ 3A.
A testing PCB is made, the DC DC booster can output 52Vdc. However, the max loading is 0.7Adc.
The circuit have sub-harmonic oscillation, when this output load is higher than 0.7A
(Yellow line = Vout, Green line = inductor current, Blue line = COMP volt, purple line = gate voltage)
the switching is normal, if the loading is 0.69A
https://1drv.ms/u/s!ApYUhFZeSAGfsgLSfYJUytsSVu3v?e=OwARQy
The circuit have sub-harmonic oscillation at loading 0.7A
https://1drv.ms/u/s!ApYUhFZeSAGfsgHxy5DfhXAH14iB?e=C9NRTc
And this is the SHC
https://1drv.ms/u/s!ApYUhFZeSAGfsgNdrXJOC5j7Ab3B?e=yLnhpS
https://1drv.ms/u/s!ApYUhFZeSAGfsgSop-Sbl39k_oQt?e=Of1zi8
Design parameter
Vin = 12.5V Lin ~ 14.2A
Vout = 52V ~ 3A
Fsw = 416Khz
L = 54uH
crossFreq is 75.9KHz, phase margin is -90 degree
Slope compensation - low pass filter 0ohm and no capacitor ( since the low pass filter made the ramp delay, it is no work for loading larger 0.14A )
it seem the the slope compensation is not effective. The result is similar, if R6's value from 100 to 825 ohm.
This is no use, when larger value of inductor- L1 (100uH and 16uH also tested) or lower current sense resistor - R17
Do you have any suggested to made it stable?
Thanks and regards
KS