This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61099: selection of inductor

Part Number: TPS61099


I'm considering 3.0V fixed type of TPS61993.
I've selected the inductor to LQM18PN1R0MFHD.
If there is concern or problem, Could you advice to me?
My product's setting is below.

Input voltage :0.7~1.5V
Output Voltage :3.0V
Output current(max) : 100mA
Typ current(typ) :500μA

I'm expecting your kindly support.