This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25947: ITIMER setting question

Part Number: TPS25947

Hi Teams,

My customer using our EVM board to verify his system and original on the EVM board is latch type(TPS259474LRPWT) is normal can do, but when he change to the TPS259474ARPW on the EVM can see his ITMER is not holding the same time with his setting from 1.83ms becomes to 1.0048ms

And his all setting as below;

First he let the R13 floating and EN pin connect to 3.3V supply.

ITIMER pin connect the 2.2nf capacitor

ILIM pin connect the 1.1Kohm(for current limited around 3A)

His load is from 0A to turn on 3.1A to see the ITIMER time.

And all these setting is the same with TPS259474LRPWT and his action is normal can meet , but why he change to TPS259474ARPW will run away the for ITIMER.

Could you help to see any issue or wrong setting from my customer ? Or the latch type and retry type of IC had different inside ?

Eddie