Hi,
I want to use LP38503ATJ-ADJ/NOPB to get 3.3V output voltage at 3A from 5V input voltage. The values specified in the datasheet of the IC are as follows:
- Input Voltage: 2.7 V to 5.5 V
- Adjustable Output Voltage: 0.6 V to 5 V
- Ensured Output Current of 3A
However, the output voltage of 3.3V at 3A cannot be designed in Webench Power Designer. What is the reason for this? It can create a circuit that can provide a maximum output current of 1.5A at 3.3V. So I can't use this IC for 3.3V output voltage at 3A? There seems to be a conflict between the datasheet and webench? I would be grateful if you answer my question. Waiting for your suggestions.